Smart autonomous solutions for farming
Maximum gain for minimum effort. Sustainable and efficient agriculture powered by HARTING's AEF high voltage interfaces.
In addition to climate change and associated extreme weather conditions, agriculture also faces additional challenges. One of them being decarbonisation to reduce the carbon footprint. The other one is demographic change with the related shortage of skilled workers. This is where autonomous solutions come in.
Precision farming for a sustainable, efficient and resilient agriculture
More time for the right farming decisions
The technology company
The mission is clearly defined: The status quo of farming should experience a revolution to ensure that sustainable agriculture can work out for everyone.
To make this happen,
Guided by smart algorithms, the autonomous robot saves time and ensures resources such as energy, fertilizer, water and seeds are used efficiently.
Autonomous tractors enable flexibility to save resources
Smart autonomous solutions for farming
AgXeed portal allows forward planning
The extreme and unpredictable weather conditions we've seen over the past years are a huge challenge for agricultural work. During the peak season, farmers need to make many critical decisions within the short term.
The
The AgXeed portal allows flexible operation planning
Smart autonomous solutions for farming
High voltage interfaces enables precision farming
Increasing the efficiency of agricultural work is one of the key factors for sustainable and resilient agriculture.
These requirements led to the common development between HARTING and partners from the agricultural environment on an equal footing. The result is the HARTING AEF high voltage interface.
A
This leads to faster configurations of agricultural machinery. The electric drive train in combination with the highly precise positioning system increase the precision of the AgBot’s work and promotes sustainability.
The HARTING AEF HV interface enables the electrification of agricultural work
Customer benefits at a glance:
Stable and flexible partnership based on common development on an equal footing
Electrification of agricultural machinery enabled by AEF high voltage interfaces
Longer lifetime thanks to interfaces suitable for harsh operating conditions (IP69K)
High reliability due to high quality standards
HARTING delivers standardised high voltage connectors, which are very well suited for the harsh operating conditions of our vehicles. The connectors are thoroughly engineered and have a very high-quality standard.
Eric Bongaerts
Manager Engineering, AgXeed