Our Technologies


Our technologies
»

Perseverance and determination are two characteristics that ensure success in any business.*

*Leo Nikolayevich Tolstoy, 1828 – 1910

We prioritise long-term corporate success over short-term flights of fancy.

Growth needs Roots

Plenty of brainpower and competent companions give us the tailwind we need on our journey:

Connectivity+ is our strategy to implement our vision "We want to shape the future with technologies for people" concretely with products and applications. Rapid technological advances, digitalisation and the demands of customers and partners have made a rethink necessary: In addition to new technologies, human and environmental factors as well as the major global issues are coming more into focus. How do we deal with all this? By thinking and acting innovatively. To take advantage of co-creation, we get customers and partners on board as early as possible. We reflect and exchange ideas, because we can only develop the best innovations for the future when we work together.

Our HARTING Quality and Technology Centre (HQT) is designed to be energy-sustainable. The architectural concept, which is based on the open campus structure, invites an open exchange of ideas. Thus, it offers the perfect environment for ensuring the long-term quality and success of the Technology Group. Because quality and technology are the essential drivers for innovation and growth.

Single Pair Ethernet (SPE) is the infrastructure foundation that makes IIoT and Industry 4.0 possible. As the IIoT market grows rapidly, we have partnered with other technology leaders to rapidly advance this technology. The SPE Industrial Partner Network provides the first point of contact for users for setting up SPE networks and devices. This partnership makes clear recommendations for developing future IIoT applications, operates a central information platform, and provides investment security for users so they can rely on this technology in the future.

Learn more Single Pair Ethernet

Together with our partners from the SmartFactory network, we have dedicated ourselves to Industry 4.0 topics and the factory of the future. Our goal, as a partnership of equals, is to advance and implement R&D projects together. The network has its own smart factory to ensure the most realistic environment possible is available.

We are part of the Microsystems Technology Laboratory (MTL) and the Microsystems Industrial Group (MIG) at the Massachusetts Institute of Technology (MIT). MTL's research areas are very broad and are helping to shape many of the next generation of Industry 4.0 technologies. As a member, we promote research and work with students and lecturers on topics relevant to Industry 4.0. For HARTING, this is an important exchange which helps us to achieve our Connectivity+ goals.

Our cooperative programme with Tongji University in Shanghai started in 2014. This cooperation includes several scholarships for the best students each year. An innovation competition is held every two years. The students' projects are evaluated by an independent jury. Since 2019, the cooperative programme has had a HARTING laboratory in which products from the transport industry are used.

»

He who stops being better stops being good

Oliver Cromwell, 1599 – 1658

We consider our technologies over the entire life cycle of the product. To ensure that our products remain sustainable, we pay attention, right from the start, to user-friendliness, critical raw materials and their recycled content. We continuously optimise our manufacturing process. Optimised shipping, packaging and recycling also helps to reduce environmental damage. Here are a few concrete examples of how we deal with environmental protection in relation to our products.

Dummy - Infographic

Starting at the development phase, we took care to design our Han Eco® in an energy-saving manner. Due to the optimised contact resistance, we are able to save almost 50 % of the energy consumed during data transmission.

HARTING Electric, Germany

We analyse our internal processes. In addition to saving time, we save up to 240 tonnes of COâ‚‚ each year by producing our cable drums directly at our Espelkamp site. The cutting process previously took place in a foreign subsidiary factory.

HARTNG Customised Solutions, Germany | HARTING Sibiu, Romania

We package using recycled foil, which consists of 85% recycled material. In this way, we reduce COâ‚‚ usage by 75.5 %, we reduce the consumption of fossil fuels by 86.6 % and we reduce our potential ozone creation by 77.2 %.

HARTING Electric | HARTING Logistics, Germany

Innovative shaped designs in die-cast aluminium and zinc, as well as optimised cooling at the contour improve the energy balance.

HARTING Applied Technologies, Germany

In regular web-seminars, we inform our customers about our products and discuss current topics. Thus, we are able to shed light on all aspects that influence the industries and our society. These aspects include simplified applications, environmental protection, and future energy concepts.

HARTING Technology Group, worldwide

The right hand for environmental protection

The right hand for environmental protection We are like Robin for Batman, Dr. Watson for Sherlock Holmes or the right hand for environmental protection. Our technologies are at home in many forward-looking markets. Whether in wind energy, rail transport or electro-mobility, our products enable sustainability and environmental protection and, thus, contribute to a clean future.

Han® S

Energy storage systems: Energy when you really need it – with the Han® S

Our Han® S was specifically developed for sustainable energy storage systems. It can be used to interconnect battery modules (BMs) to easily expand the total capacity of ESSs, which are designed on a modular basis to provide various important services. These include renewable energy integration, demand shifting and peak load reduction. By reducing peaks, it's possible to save up to 80 % on electricity expenditures.

Wind energy: Wind power switches to Ethernet

Our fibre optic transmission system serves as a matrix for Ethernet communications in modern wind turbines. We supply the complete cabling, including the rotary joint transmission. The advantage: Higher data transmission rates enable better control of the system. In addition, our Plug & Play interface ensures less downtime. Lengthy set-up times can be eliminated. System usage is optimised. That's also good for the environment!

HARTING connectors inside a wind turbine
Smart farming: Smart, smarter, AEF high voltage connector

Smart farming: Smart, smarter, AEF high voltage connector

Our AEF high voltage connector supports smart farming. The standardised connection transmits high power of 150 kW from the tractor to the implement. The electric operating mode results in improved energy efficiency compared to mechanical or hydraulic alternatives, enabling up to 20 % less diesel consumption.

E-Mobility: A charging cable for everything

A well-developed charging infrastructure with a dense network of charging stations is required for the transition to E-Mobility to be successful. That is why, in addition to vehicle charging cables, we also produce charging cables for charging stations and even charging sockets. We cover all common standards and can produce in Europe, China and the USA.

Electromobility
Avatar - female

CSR Corporate Social Responsibility

Position: Contact Person