EV Charging Cables & Connectors
The “EV Evolution” depends on long-lasting, reliable, and elegant electric vehicle charging accessories at stations around the globe.
More reliable EV charging
Since the launch of Tesla’s Model S in 2012, the automotive industry has seen an explosion of Electric Vehicle manufacturing and consumer adoption. In addition to personal vehicles, commercial and off-highway vehicles are joining the electric movement.
With more than 3.3 million EVs in use* – and millions more added each year – this revolution requires new power infrastructure to keep vehicles charged and in motion.
*as of 2023
EV charging applications
1 | At-home charging
2 | Public station charging
3 | Ultra-fast charging
4 | Mobile work station charging
The HARTING Advantage
RELIABLE CONNECTIVITY FOR NEXT-GEN DEMANDS
Reduce connector failure in harsh environments and achieve 100% uptime.
HARTING EV charging accessories are built using industrial-grade materials to withstand the abuse of motorists and the conditions of extreme heat, cold, and weather.
✓ PA66 fiberglass and thick wall design
✓ Rigorous testing processes
✓ Prevents water inundation, extreme dust, vibration or shock, reducing exposure to the elements
✓ Avoid heat loss and power waste during transfer
SLEEK DESIGN AESTHETICS
Protect your brand’s reputation and visual representation.
Function and form can work together when pairing HARTING’s EV charging connectors with your brand’s design requirements. Pack more function into less space with HARTING's proven, efficient designs.
✓ Decrease footprint without sacrificing performance
✓ Increased functionality for current and new applications
✓ Adapt to evolving industry standards
✓ Maintain brand look-and-feel
✓ Performance reliability maintains brand reputation
Meet “Buy America” Standards
The U.S. Bipartisan Infrastructure Law commits federal funding to clean transportation and energy programs. In order to qualify for these funds, manufacturers must meet several sourcing “Buy America” requirements, including:
Substantial transformation and final assembly must happen inside the U.S. Domestic assembly requirements for electric vehicle charging equipment will be effective immediately.
55% of the cost of goods sold (COGs) must be sourced from the U.S. Beginning July 1, 2024, FHWA will require that the cost of components manufactured domestically for EV charging equipment must meet the Build America, Buy America Act’s requirement of at least 55 percent domestic content for manufactured products.
HARTING’s manufacturing facilities within the U.S. and Mexico enable us to meet these “Buy America” qualifications cost-effectively.
Connect With Our Experts
Our engineers are on standby
If you’ve got questions about connectorization or our solutions' capabilities, our experts are ready to answer them.
Contact our in-house engineers for technical guidance or design help and let us be the connector specialist extension of your team.
HARTING Product Configurator
Design your next connector, then download documentation in various formats — 3D files for CAD, Bill of Materials (BOM) — for easy collaboration and hassle-free ordering.