PNO specifies HARTING ix Industrial® as new PROFINET interface
On June 29, 2021, the PROFINET User Organization (PNO) published the PROFINET Cabling and Interconnection Technology - Guideline for PROFINET Version 5.0 , a new set of rules for PROFINET-compliant cabling in industrial equipment, systems, and plants. Thanks to the ix Industrial® PROFINET are benefitting from an Ethernet interface that is significantly more compact and more robust than previous RJ45 solutions - a path to the miniaturised future. The ix Industrial® mating face for Ethernet transmission represents a key new component in the SPC "Specific Passive Components" section.
Consequently, manufacturers of PROFINET-compliant devices are now able to develop more compact devices on a secure and reliable basis and thereby save valuable installation space in the control cabinet. Given the 70% smaller ix Industrial® device socket compared to known RJ45 connections, the number of ports can be doubled for the same device size or, conversely, a device can be designed that is significantly more compact.
In addition to the miniaturisation and space savings that will become increasingly vital in the future, the HARTING ix Industrial® interface offers device manufacturers and users one thing in particular: A high-performance, reliable, and industrial-grade connector paving the way to the future.
Core properties
5.000 mating cycles
Robust metallic lock
THR shield contacts
360 degree shielding
Transmission up to 10Gbit/s
PoE/PoE+
70% smaller device socket
Benefits for PROFINET users and manufacturers:
Reliable contact in case of shock and vibration
Fewer contact interruptions
Acoustic feedback during insertion signals secure locking
Simple, convenient handling excludes accidental loosening
New miniaturisation options
Secure transmission
Depending on the application, users can choose between a straight or an angled cable outlet. This means that even tight spaces in control cabinets will not present any problems. Catering to demanding environments, the ix Industrial® interface will also be available in IP65/67 protected PushPull housings as from the autumn.
Measurement technology manufacturers established on the markets are reliably supporting the ix Industrial® standard with a wide range of measurement technology.
More
Jonas Diekmann
Position: Technical editor
- Department: Global Product Management
- Company: HARTING Electronics GmbH